Everything

Connecting a Debugger and Downloading

In this section, you debug the program using E1.First, make preparation for debugging.

 

1. Selecting a debug tool

In this step, you select [RH850 E1(LPD) (Debug Tool)] as a debug tool to be used.

Right-click on the Debug Tool in the Project Tree and select [Using Debug Tool] > [RH850 E1(LPD)(Debug Tool)].

[RH850 E1(LPD)] is selected as a debug tool.