Everything

Editing the Program

In this section, the basic editing method is explained.

First, the basic editing method is explained, and then you edit the program through a simple copy and paste procedure. Edit the program following the steps listed below.

 

1. How to open a source code file

The following step describes how to open a source code file.

 

Find the source code file you want to edit in the Project Tree and double-click it.

This displays the source code in the Main panel.