D.2  Displaying Icons at Locations of Input Errors
 
In some of the panels and dialog boxes provided by CS+, the 
 icon will appear at a point where incorrect characters are entered or a required item is missing.
Remark  | Placing the cursor over the  
 icon will pop up the information that indicates the characters to be entered (tips to fix the error).  | 
 
Figure D.1  | Sample Icons Shown at Locations of Input Errors  |