Everything

Chart Visualization Chooser dialog box


This dialog box specifies the type of state line to be displayed as an execution transition of the processing program, and whether an event mark is or is not to be displayed as a real-time OS resource usage status, in the Analysis information diagram area on the Analysis Result panel.

Figure A.9

Chart Visualization Chooser Dialog Box

 

The following items are explained here.

[How to open]

-

Press the button located on the Toolbar on the Analysis Result panel.

[Description of each area]

(1)

State line select area

Selects whether or not to display the applicable state line or event mark in the Analysis information diagram area on the Analysis Result panel.

Checked

Displays the applicable state line or event mark in the Analysis information diagram area on the Analysis Result panel.

Not checked

Hides the applicable state line or event mark from the Analysis information diagram area on the Analysis Result panel.

[Function buttons]

Default

Resets the type of state line to be displayed and whether an event mark is or is not to be displayed in the Analysis information diagram area on the Analysis Result panel to its default condition.

Close

Closes this dialog box.