The features of the build tool plug-in are shown below.
Most build options can be set via the graphical user interface (GUI).
Two types of facilities are provided to speed up build: simultaneous build and parallel build.
The build time can be shortened in simultaneous build by simultaneously compiling or assembling the files with a single call of the build command and in parallel build by executing multiple build commands in parallel.