This tab shows the detailed information on a C++ source file categorized by the following and the configuration can be changed.
Note that this tab takes over the settings of the [Common Options] tab and [Compile Options] tab.
When the settings are changed from these tabs, the properties are displayed in boldface.
When [Yes] in the [Set individual compile option] property in the [Build] category from the [Build Settings] tab is selected |
When [Always latest version which was installed] or V1.12.00 or a later version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.12.00 or a later version of the CC-RL compiler has been installed |
[Description of each category]
The detailed information on debug information is displayed and the configuration can be changed.
Select whether to generate the debug information. It is possible to perform source debugging with the debugger by outputting information for source debugging to the output file. This property corresponds to the -g option of the ccrl command. |
||||||
Select whether to enhance debug information at optimization. This property corresponds to the -g_line option of the ccrl command. This property is displayed in the following cases.
|
||||||
The detailed information on the optimization is displayed and the configuration can be changed.
The detailed information on the optimization is displayed and the configuration can be changed.
Specify the maximum number of times to expand the loops such as "for" and "while". If 0 or 1 is specified, expansion is suppressed. If this is blank, the -Ounroll option is not added to the command line. In this case, a value in accordance with the selection of the [Level of optimization] property is used by the compiler. This property corresponds to the -Ounroll option of the ccrl command. This property is displayed only when [Perform the default optimization(No option specified)], [Code size precedence(-Osize)] or [Speed precedence(-Ospeed)] in the [Level of optimization] property is selected. |
||||||||||
Select whether to remove the static functions which are not called. This property corresponds to the -Odelete_static_func option of the ccrl command. |
||||||||||
Performs optimization according to the [Level of optimization] property. |
||||||||||
Does not remove the unused static functions which are not called. |
||||||||||
Specify whether to perform inline expansion at the location calling functions. This property corresponds to the -Oinline_level option of the ccrl command. This property is displayed only when [Perform the default optimization(No option specified)], [Code size precedence(-Osize)], [Speed precedence(-Ospeed)] or (*1) [Partial optimization(-Olite)] in the [Level of optimization] property is selected. *1 When [Always latest version which was installed] or V1.12.00 or a later version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.12.00 or a later version of the CC-RL compiler has been installed. |
||||||||||
Performs optimization according to the [Level of optimization] property. |
||||||||||
Performs inline expansion at the location calling the function for which #pragma inline is specified. |
||||||||||
Yes(Auto-detect, to specify maximum increasing rate)(-Oinline_level=2 -Oinline_size) |
Distinguishes the function that is the target of inline expansion automatically and expands it. Specify the maximum rate of increase. |
|||||||||
Yes(Auto-detect, maximum increasing rate : to adjust the level of optimization)(-Oinline_level=2) |
Distinguishes the function that is the target of inline expansion automatically and expands it. The compiler takes a value that suits the optimization level as the maximum rate of increase. |
|||||||||
Yes(Auto-detect without code size increase)(-Oinline_level=3) |
Distinguishes the function that is the target of inline expansion automatically and expands it, while minimizing the increase in code size. |
|||||||||
Suppresses all inline expansion including the function for which "#pragma inline" is specified. |
||||||||||
Specify the maximum increasing rate (%) of the code size up to which inline expansion is performed. (Example: When "100" is specified, inline expansion will be applied until the code size increases by 100% (becomes twice the initial size).) This property corresponds to the -Oinline_size option of the ccrl command. This property is displayed when [Yes(Auto-detect, to specify maximum increasing rate)(-Oinline_level=2 -Oinline_size)] in the [Perform inline expansion] property is selected, or when [To adjust the level of optimization(No option specified)] in the [Perform inline expansion] property and [Speed precedence(-Ospeed)] in the [Level of optimization] property are selected. |
||||||||||
Select whether to improve the program's execution performance by reordering instructions at the machine-language level. This property corresponds to the -Opipeline option of the ccrl command. This property is displayed only in the following cases.
|
||||||||||
Performs optimization according to the [Level of optimization] property. |
||||||||||
Use br instruction to call a function at the end of the function |
Select whether to give precedence to using br instructions in the place of call instructions when the function ends with a function call. This property corresponds to the -Otail_call option of the ccrl command. |
|||||||||
Performs optimization according to the [Level of optimization] property. |
||||||||||
Gives precedence to using br instructions in the place of call instructions when the function ends with a function call. The code size can be reduced by removing the ret instruction. |
||||||||||
Uses call instructions when the function ends with a function call. |
||||||||||
Select whether to create a subroutine for the same instruction sequence. This property corresponds to the -Osame_code option of the ccrl command. This property is displayed in the following cases.
|
||||||||||
Performs optimization according to the [Level of optimization] property. |
||||||||||
Does not create a subroutine for the same instruction sequence. |
||||||||||
Select whether to reduce the code size of the relative branch instructions. This property corresponds to the -Obranch_chaining option of the ccrl command. This property is displayed only when [Perform the default optimization(No option specified)] or [Code size precedence(-Osize)] in the [Level of optimization] property is selected. |
||||||||||
Performs optimization according to the [Level of optimization] property. |
||||||||||
Does not reduce the code size of the relative branch instructions. |
||||||||||
Select whether to proceed with optimization through a change of the alignment conditions. This property corresponds to the -Oalign option of the ccrl command. This property is displayed in the following cases.
|
||||||||||
Performs optimization according to the [Level of optimization] property. |
||||||||||
Performs optimization through a change of the alignment conditions. |
||||||||||
Does not perform optimization through a change of the alignment conditions. |
||||||||||
Outputs additional information for inter-module optimization |
Select whether to output additional information for inter-module optimization. At linkage, inter-module optimization is applied to files for which this option has been specified. This property corresponds to the -goptimize option of the ccrl command. |
|||||||||
Outputs additional information for inter-module optimization. |
||||||||||
Does not outputs additional information for inter-module optimization. |
The detailed information on preprocessing is displayed and the configuration can be changed.
Specify the additional include paths during compiling. The following placeholders are supported. %ActiveProjectDir%: Replaces with the absolute path of the active project folder. %ActiveProjectName%: Replaces with the active project name. %BuildModeName%: Replaces with the build mode name. %MainProjectDir%: Replaces with the absolute path of the main project folder. %MainProjectName%: Replaces with the main project name. %MicomToolPath%: Replaces with the absolute path of the install folder of this product. %ProjectDir%: Replaces with the absolute path of the project folder. %ProjectName%: Replaces with the project name. %TempDir%: Replaces with the absolute path of the temporary folder. %WinDir%: Replaces with the absolute path of the Windows system folder. The specified include path is searched with higher priority than the standard include file folder of CC-RL. The reference point of the path is the project folder. When this property is omitted, only the standard folder of CC-RL is searched. This property corresponds to the -I option of the ccrl command. The specified include path is displayed as the subproperty. Uppercase characters and lowercase characters are not distinguished for the include paths. |
||||||||
Edit by the Path Edit dialog box which appears when clicking the [...] button. For the subproperty, you can enter directly in the text box. |
||||||||
Select whether to compile using the include path specified in the [Additional include paths] property in the [Preprocess] category from the [Compile Options] tab of the build tool to be used. The include paths are added by the following procedure.
This property corresponds to the -I option of the ccrl command. |
||||||||
Compiles using the include path specified in the property of the build tool to be used. |
||||||||
Does not use the include path specified in the property of the build tool to be used. |
||||||||
Specify the file that is included at the top of the compilation unit. The following placeholders are supported. %ActiveProjectDir%: Replaces with the absolute path of the active project folder. %ActiveProjectName%: Replaces with the active project name. %BuildModeName%: Replaces with the build mode name. %MainProjectDir%: Replaces with the absolute path of the main project folder. %MainProjectName%: Replaces with the main project name. %MicomToolPath%: Replaces with the absolute path of the install folder of this product. %ProjectDir%: Replaces with the absolute path of the project folder. %ProjectName%: Replaces with the project name. %TempDir%: Replaces with the absolute path of the temporary folder. %WinDir%: Replaces with the absolute path of the Windows system folder. The reference point of the path is the project folder. This property corresponds to the -preinclude option of the ccrl command. The specified include file name is displayed as the subproperty. |
||||||||
Edit by the Text Edit dialog box which appears when clicking the [...] button. For the subproperty, you can enter directly in the text box. |
||||||||
Specify the name of the macro to be defined. Specify in the format of "macro name=defined value", with one macro name per line. The "=defined value" part can be omitted, and in this case, "1" is used as the defined value. This property corresponds to the -D option of the ccrl command. |
||||||||
Edit by the Text Edit dialog box which appears when clicking the [...] button. For the subproperty, you can enter directly in the text box. |
||||||||
Specify the macro name to be undefined. Specify in the format of "macro name", with one macro name per line. This property corresponds to the -U option of the ccrl command. |
||||||||
Edit by the Text Edit dialog box which appears when clicking the [...] button. For the subproperty, you can enter directly in the text box. |
||||||||
The detailed information on the source is displayed and the configuration can be changed.
The language of the C source file. This property corresponds to the -lang option of the ccrl command. |
||||
The detailed information on character encoding is displayed and the configuration can be changed.
The character encoding to be used for Japanese/Chinese comments and character strings in the C++ source file. This property corresponds to the -character_set option of the ccrl command. |
||||
The detailed information on output code is displayed and the configuration can be changed.
Select the code output mode for switch statements in programs. This property corresponds to the -switch option of the ccrl command. |
||||
Outputs the switch statements in the same format as the if-else statement along a string of case statements in programs. Select this item if the case statements are written in the order of frequency or if only a few labels are used. Because the case statements are compared starting from the top, unnecessary comparison can be reduced and the execution speed can be increased if the case statement that most often matches is written first. |
||||
Outputs the code in the binary search format for switch statements in programs. Searches for a matching case statement by using a binary search algorithm. If this item is selected when many labels are used, any case statement can be found at almost the same speed. |
||||
Outputs the code in the table jump format (absolute branch) for switch statements in programs. References a table indexed on the values in the case statements, and selects and processes case labels from the switch statement values. The code will branch to all the case statements with about the same speed. However, if case values are not used in succession, an unnecessary area will be created. |
||||
Outputs the code in the table jump format (relative branch) for switch statements in programs. References a table indexed on the values in the case statements, and selects and processes case labels from the switch statement values. The code will branch to all the case statements with about the same speed. However, if case values are not used in succession, an unnecessary area will be created. |
||||
Select whether to output a C++ source program as a comment to the assembly source file to be output. This property corresponds to the -pass_source option of the ccrl command. This property is displayed only when [Yes(-asm_path)] in the [Output assembly source file] property in the [Output File] category is selected or when [Yes(-asmopt=-prn_path)] in the [Output assemble list file] property in the [Assemble List] category is selected. |
||||
Outputs a C++ source program as a comment to the assembly source file. |
||||
Does not output a C++ source program as a comment to the assembly source file. |
The detailed information on output files is displayed and the configuration can be changed.
The detailed information on the assemble list is displayed and the configuration can be changed.
The detailed information on the error output is displayed and the configuration can be changed.
Select whether to output the error message file. This property corresponds to the -error_file option of the ccrl command. Error messages are displayed on the Output panel regardless of this property's. This property is displayed only when [No] in the [Build in parallel] property in the [Build Method] category from the [Common Options] tab is selected |
||||
Specify the folder which the error message file is output. If a relative path is specified, the reference point of the path is the main project or subproject folder. If an absolute path is specified, the reference point of the path is the main project or subproject folder (unless the drives are different). The following placeholder is supported. %BuildModeName%: Replaces with the build mode name. If this is blank, it is assumed that the project folder has been specified. This property corresponds to the -error_file option of the ccrl command. This property is displayed only when [Yes(-error_file)] in the [Output error message file] property is selected. |
||||
Directly enter in the text box or edit by the Browse For Folder dialog box which appears when clicking the [...] button. |
||||
Specify the error message file name. The extension can be freely specified. The following placeholders are supported. %ActiveProjectName%: Replaces with the active project name. %MainProjectName%: Replaces with the main project name. %ProjectName%: Replaces with the project name. If this is blank, it is assumed that "%ProjectName%.err" has been specified. This property corresponds to the -error_file option of the ccrl command. This property is displayed only when [Yes(-error_file)] in the [Output error message file] property is selected. |
||||
The detailed information on warning messages is displayed and the configuration can be changed.
The detailed information on messages is displayed and the configuration can be changed.
Select whether to change the type of warning messages to error. This property corresponds to the -change_message option of the ccrl command. This property is displayed when [Always latest version which was installed] or V1.06.00 or a later version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.06.00 or a later version of the CC-RL compiler has been installed. |
||||||
Yes(Specify message number)(-change_message=error=<Message number>) |
Specifies the number of warning message of which type is to be changed to error. |
|||||
Specify the number of the warning message. If multiple message numbers are specified, delimit them with "," (comma) (example: 23028,23086). Also, a range of message numbers can be specified using "-" (hyphen) (example:23028-23086). This property corresponds to the -change_message option of the ccrl command. This property is displayed only in the following cases.
|
||||||
Directly enter in the text box or edit by the Character String Input dialog box which appears when clicking the [...] button. |
||||||
Other detailed information on compilation is displayed and the configuration can be changed.