Everything
2.4.2 Perform optimization with the execution speed precedence

Select the build tool node on the project tree and select the [Compile Options] tab on the Property panel.

To perform optimization with the execution speed precedence, select [Speed precedence(-Ospeed)] in the [Level of optimization] property in the [Optimization] category.

Figure 2.18

[Level of optimization] Property (Execution Speed Precedence)

Remark

You can also set the option in the same way with the [Level of optimization] property in the [Frequently Used Options(for Compile)] category on the [Common Options] tab.