Everything
2.2.2 Output map information

The map information (the information of the link result) is output to the map file.

Select the build tool node on the project tree and select the [Link Options] tab (for the application project) or [Create Library Options] tab (for the library project) on the Property panel.

To output the map file, select [Generate Default Map File(-map)] in the [Map File Generation] property in the [List] category.

Figure 2.5

[Map File Generation] Property

 

The map file is output to the folder specified in the [Output folder] property.

The file name will be the output file name of the linker with the extension replaced by ".map".