Everything
A.1 Description

The following lists the panels/dialog boxes used in the build tool.

Table A.1

List of Panels/Dialog Boxes

Panel/Dialog Box Name

Function Description

Property panel

This panel is used to display the detailed information on the Build tool node or file that is selected on the Project Tree panel and change the settings of the information.

System Include Path Order dialog box

This dialog box is used to refer the system include paths specified for the compiler and set their specified sequence.

Select Modules Which Are Output in Files dialog box

This dialog box is used to set modules which are output to the I/O header file.