Everything
4.1 Message Formats

The output formats of messages are as follows.

 

-

When the file name and line number are included

-

Message number type is information

file-name (line-number):message-number:[information-type] message

The information type is change, insertion, deletion, or information.

 

-

Message number type is other than information

file-name (line-number):message-number:message

 

-

When the file name and line number are not included

message-number:message

 

The message number is output as a consecutive string consisting of one alphabetic character, 0591, and a three-digit number.