The RH850 Code Generator tool has the following original spec.
The RH850 Code Generator tool output synchronization processing in Create and Stop of each peripherals. The user has to edit synchronization processing.
The RH850 Code Generator tool can not edit interrupt vector table. When using generated interrupt function, please edit interrupt vector table.(Target device : RH850/E1L, E1M-S)
The Code Generator install folder has SampleProjects folder. This folder has sample project.