Performs processing in response to the transfer end interrupt.
Remark The API function is called as the interrupt process corresponding to the DMA transfer end interrupt for channel n
[Syntax]
static void r_dmac_dmacni_interrupt ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.