Sets the value for comparison with, addition to, or subtraction from the reference value.
[Syntax]
void R_DOC_WriteData ( uint16_t data );
[Argument(s)]
I/O
Argument
Description
I
uint16_t data;
Input data for use in operation
[Return value]
None.