Performs processing in response to the floating-point exception.
Remark This API function is called to run interrupt processing in response to a floating-point exception occurred when detecting the five exception events (overflow, underflow, inexact, division-by-zero, and invalid operation) specified in the IEEE754 standard and another floating-point exception that is generated on detection of unimplemented processing.
[Syntax]
void r_floatingpoint_exception ( void );
[Argument(s)]
None.
[Return value]
None.