Sets the clock source that is selected following release from sleep mode.
[Syntax]
#include "r_cg_macrodriver.h"
#include "r_cg_lpc.h"
MD_STATUS R_LPC_ChangeSleepModeReturnClock ( return_clock_t clock );
[Argument(s)]
I/O |
Argument |
Description |
I |
return_clock_t clock; |
Clock source type RETURN_LOCO : Low-speed on-chip oscillator RETURN_HOCO : High-speed on-chip oscillator RETURN_MAIN_CLOCK : Main clock oscillator RETURN_DISABLE : Switching of the clock source does not proceed. |
[Return value]
Macro |
Description |
MD_OK |
Normal completion |
MD_ERROR1 |
Change to the low-speed operating mode ended abnormally. |
MD_ARGERROR |
Invalid argument clock specification |