Everything

r_s12adn_interrupt

Performs processing in response to the A/D scan end interrupt.

Remark         This API function is called to run interrupt processing for the A/D scan end interrupt, which is generated on completion of scanning of the analog inputs.

 

[Syntax]

static void    r_s12adn_interrupt ( void );

Remark         n is the unit number.

 

[Argument(s)]

None.

 

[Return value]

None.