Performs processing in response to the transmit-end interrupts.
Remark This API function is called to run the interrupt processing for the transmit-end interrupt.
[Syntax]
static void r_scifan_teif_interrupt ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.