When performing code generation, if you enter an invalid string in the Peripheral Functions panel, or a required input is missing, then a icon displays next to the incorrect input, and the text is displayed in red to warn that there is a problem with the input.