Everything

det_mem

Outline
Unregister memory object.
C format
 ER      det_mem (VP base);
Parameter(s)
I/O
Parameter
Description
I
 VP      base;
Memory object start address.

Explanation
This service call can be called from tasks that belong to Trusted Domain.
This service call unregisters the memory object started from the address specified by base.
Return value
Macro
Value
Description
E_OK
0
Normal completion.
E_CTX
-25
Context error.
- This service call was issued in the CPU locked state.
- This service call was issued from non-task.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
E_MACV
-26
Memory access violation.
- Stack pointer points out of user stack for invoking task.
E_OACV
-27
Object access violation.
- The invoking task does not belong to trusted domain.
E_NOEXS
-42
Non-existent object.
- The memory object started from the address specified by base has already been registered.