rel_wai
irel_wai
ER rel_wai (ID tskid);
ER irel_wai (ID tskid);
 As a result, the target task unlinked from the wait queue and is moved from the WAITING state to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
 "E_RLWAI" is returned from the service call that triggered the move to the WAITING state (slp_tsk, wai_sem, or the like) to the task whose WAITING state is cancelled by this service call.
 Note 1	 These service calls do not perform queuing of forced cancelation requests. If the target task is neither in the WAITING state nor WAITING-SUSPENDED state, "E_OBJ" is returned.