-
sns_tex
-
Reference task exception disabled state.
BOOL sns_tex (void);
This service call returns TRUE if the task in the RUNNING state is in the task exception disabled state, and otherwise
Table 19-7 Return value of sns_tex
Task in the RUNNING state
|
Task exception handling routine for the task in the RUNNING state
|
Task exception disabled state for the task in the RUNNING state
|
|
|
|
|
|
|
|
|
|
|
|
|
|
When task exception handling routine is not defined, task exception handling is disabled.
|
|
|
|
|
|
|
|
|
|
|
Normal completion (task exception disabled state).
|
|
|
Normal completion (task exception enabled state).
|
|
|
- This service call was issued in the status PSW.IPL > kernel interrupt mask level.
|