-   
 
   vsys_dwn
   ivsys_dwn
  
    -   
  
 
 void    vsys_dwn(W type, VW inf1, VW inf2, VW inf3);
 void    vsys_dwn(W type, VW inf1, VW inf2, VW inf3);
 
  
  
    | 
 | 
    
 | 
    
 | 
  
  
    | 
 | 
    
 W     type;
 
 | 
    
 | 
  
  
    | 
 | 
    
 VW    inf1;
 
 | 
    
 System down information 1
  
 | 
  
  
    | 
 | 
    
 VW    inf2;
 
 | 
    
 System down information 2
  
 | 
  
  
    | 
 | 
    
 VW    inf3;
 
 | 
    
 System down information 3
  
 | 
  
 
 Specify the value (from 1 to 0x7FFFFFFF) typed to the occurring error for 
type. Note the value of 0 or less is reserved by the RI600PX.
 
 These service calls never return.
 
 These service calls are the function outside the range of 
mITRON4.0 specifications.
 
 Note	 The system down routine is also called when abnormality is detected in the RI600PX.