[System Configuration File Related Information] tab
This tab shows the detailed information on the using system configuration file categorized by the following and the configuration can be changed.
The detailed information on the RI600V4 generation files are displayed and the configuration can be changed.
When an undefined interrupt occurs, the system down is caused. When -U option is specified, the vector number will be transferred to the system down routine (refer to "CAHPTER 13SYSTEM DOWN"). This is useful for debugging. However, the kernel code size increases by about 1.5 KB.
|
||||
Specify the path where the table generation utility mkritbl retrieves the service call information files.
Specifies the service call information file (.mrc) or the path to the folder where the service call information files are retrieved.
|
||||
Note 1 Refer to "2.6.1 Service call information files and "-ri600_preinit_mrc" compiler option" for the service call information file.