13.3.3 Clock timer interrupt source
Define the following items as clock timer interrupt source information:
Only one information item can be defined as clock timer interrupt source information
The following shows the clock timer interrupt source information format.
The items constituting clock timer interrupt source information are as follows.
1 ) Clock timer interrupt source:
tim_intno
Specifies the interrupt source for a clock timer.
Only interrupt source names prescribed in the device file or only values from 0x0 to 0x7c can be specified.
If an interrupt source name is specified for
tim_intno, the CF78V4 activation option -cpu
D <name> must be