13.4.3 Eventflag information
The number of eventflag information items that can be specified is defined as being within the range of 0 to 127.
Note The CF78V4 outputs to the system information header file the correspondence between the eventflag names and IDs, in the following format. Consequently, eventflag names can be used in the place of IDs by including the relevant system information header file using the processing program.
Specifies the attributes (queuing method, queuing count, clear) of the eventflag.
The keywords that can be specified for flgatr are TA_TFIFO, TA_WSGL and TA_CLR.
The keywords that can be specified for flgatr are TA_TFIFO, TA_WSGL and TA_CLR.
TA_TFIFO: If the bit pattern of the eventflag does not satisfy the required condition when wai_flg or twai_flg is issued, the task is queued to the eventflag wait queue.