Everything

can_act

Outline
Cancel task activation requests.
C format
 ER_UINT can_act ( ID tskid );

Assembly format
 MOV     A, #tskid
 CALL    !!_can_act

Parameter(s)
I/O
Parameter
Description
I
 ID      tskid;
ID number of the task for cancelling activation requests.
TSK_SELF: Invoking task.
Value: ID number of the task for cancelling activation requests.

Explanation
This service call cancels all of the activation requests queued to the task specified by parameter tskid (sets the activation request counter to 0x0).
When this service call is terminated normally, the number of cancelled activation requests is returned.
Return value
Macro
Value
Description
-
-
Normal completion (activation request count: positive value or 0).