frsm_tsk
ifrsm_tsk
These service calls set the suspend request counter for the task specified by parameter tskid to 0x1 f, and then forcibly cancel the SUSPENDED state of the target task.
As a result, the target task is moved from the SUSPENDED state to the READY state, or from the WAITING-SUSPENDED state to the WAITING state.
Note 1 If the target task is moved to the READY state after this service call is issued, this service call also re-queues the task at the end of the ready queue corresponding to the priority of the task.