fsnd_dtq
ifsnd_dtq
MOVW DE, !LOWW(_data+0x00002) MOVW BC, !LOWW(_data) MOV A, #dtqid CALL !!_fsnd_dtq MOVW DE, !LOWW(_data+0x00002) MOVW BC, !LOWW(_data) MOV A, #dtqid CALL !!_ifsnd_dtq |
These service calls write data specified by parameter data to the data queue area of the data queue specified by parameter dtqid.
If there is no available space for writing data in the data queue area of the target data queue when either of these service calls is issued, the service call overwrites data to the area with the oldest data that was written.
If a task has been queued to the reception wait queue of the target data queue when this service call is issued, this service call does not write data but transfers the data to the task. As a result, the task is unlinked from the reception wait queue and moves from the WAITING state (data reception wait state) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.