Everything

stp_cyc

Outline
Stop cyclic handler operation.
C format
 ER      stp_cyc ( ID cycid );

Assembly format
 MOV     A, #cycid
 CALL    !!_stp_cyc

Parameter(s)
I/O
Parameter
Description
I
 ID      cycid;
ID number of the cyclic handler operation to be stopped.

Explanation
This service call moves the cyclic handler specified by parameter cycid from the operational state (STA state) to non-operational state (STP state).
As a result, the target cyclic handler is excluded from activation targets of the RI78V4 until issuance of sta_cyc.
Note This service call does not perform queuing of stop requests. If the target cyclic handler has been moved to the non-operational state (STP state), therefore, no processing is performed but it is not handled as an error.
Return value
Macro
Value
Description
E_OK
0
Normal completion.