chg_pri
ichg_pri
ER chg_pri (ID tskid, PRI tskpri);
ER ichg_pri (ID tskid, PRI tskpri);
 These service calls change the priority of the task specified by parameter tskid (current priority) to a value specified by parameter tskpri.
 If the target task is in the RUNNING or READY state after this service call is issued, this service call re-queues the task at the end of the ready queue corresponding to the priority specified by parameter tskpri, following priority change processing.
 Note	 When the target task is queued to a wait queue in the order of priority, the wait order may change due to issue of this service call.
 Example	 When three tasks (task A: priority level 10, task B: priority level 11, task C: priority level 12) are queued to the semaphore wait queue in the order of priority, and the priority level of task B is changed from 11  to 9, the wait order will be changed as follows.