pget_mpf
ipget_mpf
ER pget_mpf (ID mpfid, VP *p_blk);
ER ipget_mpf (ID mpfid, VP *p_blk);
This service call acquires the fixed-sized memory block from the fixed-sized memory pool specified by parameter mpfid and stores the start address in the area specified by parameter p_blk.
If a fixed-sized memory block could not be acquired from the target fixed-sized memory pool (no available fixed-sized memory blocks exist) when this service call is issued, fixed-sized memory block acquisition processing is not performed but "E_TMOUT" is returned.
Note 1 The RI850V4 does not perform memory clear processing when acquiring a fixed-sized memory block. The contents of the acquired fixed-sized memory block are therefore undefined.
Note 2 If no fixed-size memory blocks could be acquired from the target fixed-size memory pool (no available fixed-size memory blocks exist) when this service call is issued, the contents in the area specified by parameter p_blk become undefined.