Everything

 

-Xpreinclude


This option specifies the file that is included at the top of the compilation unit.

[Specification format]

-Xpreinclude=file[,file]...

 

-

Interpretation when omitted

It is assumed that the file that is included at the top of the compilation unit does not exist.

[Detailed description]

-

This option specifies the file that is included at the top of the compilation unit as file.

-

This option starts searching from the folder that started the complier if the file is specified by its relative path.

[Example of use]

-

To include file "sample.h" at the top of the compilation unit, describe as:

>ccrh main.c -Xpreinclude=sample.h -Xcommon=rh850