Everything

 

@


This option specifies a subcommand file.

[Specification format]

@file

 

-

Interpretation when omitted

Only the options and file names specified on the command line are recognized.

[Detailed description]

-

This option handles file as a subcommand file.

-

An error will occur if file does not exist.

-

An error will occur if file is omitted.

-

See "2.4.2 Subcommand file usage" for details about a subcommand file.

[Example of use]

-

To handle "command.txt" as a subcommand file, describe as:

>ccrh @command.txt -Xcommon=rh850