Everything

 

-h


This option displays the descriptions of asrh options.

[Specification format]

-h

 

-

Interpretation when omitted

The descriptions of asrh options are not displayed.

[Detailed description]

-

This option outputs the descriptions of asrh options to the standard error output.
It does not execute assembling.

[Example of use]

-

To output the descriptions of asrh options to the standard error output, describe as:

>asrh -h -Xcommon=rh850