Everything

 

-Xprn_path


This option specifies the folder to save the assemble list file.

[Specification format]

-Xprn_path[=path]

 

-

Interpretation when omitted

An assemble list file will not be output.

[Detailed description]

-

This option specifies the folder to save the assemble list file output during assembling as path.

-

If an existing folder is specified as path, the assemble list file is saved under the source file name with the extension replaced by ".prn" to path.
An error will occur if a nonexistent folder is specified.

-

An existing file can be specified as path.

-

The assemble list file is saved with path as the file name.
An error will occur if a nonexistent file is specified.

-

If "=path" is omitted, the assemble list file is saved to the current folder under the source file name with the extension replaced by ".prn".

[Example of use]

-

To save the assemble list file output during assembling to folder "D:\sample", describe as:

>asrh -Xprn_path=D:\sample -Xcommon=rh850 main.asm