Everything

.dbl_size [V2.04.00 or later]


Embeds the information of the -Xdbl_size option of the compiler into the object.

[Syntax]

Symbol field

Mnemonic field

Operand field

Comment field

 
.dbl_size
size-value
[; comment]

[Function]

-

The .dbl_size directive embeds the information of the -Xdbl_size option of the compiler into the object.

[Description]

-

This directive embeds the information of the -Xdbl_size option of the compiler into the object.

-

This directive does not affect the operation of the .float and .double directives.