Initialization of 4-byte area.
The .float directive also tells the assembler to initialize a memory area in 4-byte units with the absolute-expression specified in the operand field. |
The value of the absolute expression is allocated as a single-precision floating-point number. Consequently, the value of the expression must be between -3.40282347e+38 and 3.40282347e+38. In other cases, it is assumed as infinity with the same sign. |
If the relocation attribute of the section is "BSS", then an error is output because the .float directive cannot be described. |