The peripheral device initialization function is as follows.
Table 7.15
Peripheral Device Initialization Function
Function/Macro Name
Outline
hdwinit
Initialization of peripheral devices immediately after the CPU reset