"path" specified by the "character string" option is a file. Specify a folder. |
||
The folder "folder" specified by the "character string" option is not found. |
||
The "character string2" option is ignored when the "character string1" option is specified at the same time. |
||
The "-Xfloat" option is ignored because specified device does not have FPU. |
||
"symbol name" specified in the "character string" option is not allowed for a preprocessor macro. |
||
The "character string" option is specified more than once. The latter is valid. |
||
The "character string2" option is ignored when the "character string1" option and the "character string2" option are inconsistent. |
||
The "character string2" option is ignored when the "character string1" option is not specified. |
||
Optimization itemoptions were cleared when "-Ocharacter string" option is specified. Optimization itemoptions need to specify after "-Ocharacter string" option. |
||
The same file name was specified more than once in a command line. CC-RH is not capable of handling multiple instances of the same file name. |
||
The evaluation version is valid for the remaining number days. |
||
The license manager is not installed. Install the correct license manager. |
||
The "-g" option is effective because the "option" option is specified. |
||
Explicitly specify the "-g" option to suppress output of this message. |
||
The trial period for the features of the Professional edition expires in number days. Please consider purchasing the product of Professional edition. |
||
Type qualifiers are meaningless in this declaration. Ignored. |
||
Too many characters in character constant. Character constants cannot contain more than one character. |
||
Since there is a preceding #else, this directive is illegal. |
||
Storage class is not first. Specify the declaration of the storage class first. |
||
Declaration is incompatible with "declaration" (declared at line number). |
||
Argument of type "type1" is incompatible with parameter of type "type2". |
||
External/internal linkage conflict with previous declaration. |
||
Floating-point value does not fit in required integral type. |
||
Integral value does not fit in required floating-point type. |
||
Floating-point value does not fit in required floating-point type. |
||
Declaring a void parameter list with a typedef is nonstandard. |
||
A value of type name1 cannot be assigned to an entity of type name2. |
||
Transfer of control bypasses initialization of: type "symbol" (declared at line number). |
||
Using out-of-scope declaration of type "symbol" (declared at line number). |
||
Declaration of "size_t" does not match the expected type name. |
||
Missing return statement at end of non-void function "name". |
||
A universal character name cannot designate a character in the basic character set. |
||
Subtraction of pointer types "type name1" and "type name2" is nonstandard. |
||
Standard requires that name be given a type by a subsequent declaration ("int" assumed). |
||
Constant is too large for long long; given unsigned long long type (nonstandard). |
||
Multicharacter character literal (potential portability problem). |
||
Definition at end of file not followed by a semicolon or a declarator. |
||
The declaration at the end of the file lacked a semicolon to indicate its termination. |
||
White space is required between the macro name "macro name" and its replacement text |
||
Insert a space between the macro name and the text to be replaced. |
||
Using "function item" function at influence the code generation of "SuperH" compiler |
||
The use of "function item" may affect compatibility with the SuperH compiler. Confirm details of differences in the specification. |
||
argument is incompatible with formal parameter of intrinsic function |
||
const qualifier for variable "variable-name" differs between files. |
||
Illegal displacement.Only the effective lower-order digits will be recognized as being specified, and the assembly will continue. |
||
Illegal operand (range error in immediate). Only the effective lower-order digits will be recognized as being specified, and the assembly will continue. |
||
Only the effective lower-order digits will be recognized as being specified, and the assembly will continue. |
||
Only the effective lower-order digits will be recognized as being specified, and the assembly will continue. |
||
Illegal register number, ignored. The invalid register will be ignored, and the assembly will continue. |
||
string already specified, ignored. The previously specified number will be used. This specification will be ignored. |
||
Illegal register number, aligned odd register(rXX) to be even register(rYY). |
||
Odd-numbered registers (r1, r3, ... r31) have been specified. The only general-purpose registered that can be specified are even-numbered (r0, r2, r4, ... r30). Assembly will continue, assuming that even-numbered registers (r0, r2, r4, ... r30) have been specified. |
||
Duplicated reg_mode, ignored $REG_MODE. The "-Xreg_mode" option takes precedence, and register modes specified via the $REG_MODE control instruction will be ignored. |
||
option1 and option2 cannot be specified simultaneously. option1 is ignored. |
||
option and the option to divide the output file cannot be specified simultaneously. option is ignored. The first input file name is used as the output file name. |
||
Fatal level message cannot be changed to other level : "option" |
||
The level of an fatal error message cannot be changed. The specification of option is ignored. Only messages at the information/warning/error level can be changed with the change_message option. |
||
Subcommand file terminated with end option instead of exit option |
||
There is no processing specification following the end option. Processing is done with the exit option assumed. |
||
Duplicate specifications of option were found. Only the last specification is effective. |
||
option was used to specify the same file twice. The second specification is ignored. |
||
option was used to specify the same module twice. The second specification is ignored. |
||
Duplicate symbol/section specified in option "option" : "name" |
||
option was used to specify the same symbol name or section name twice. The second specification is ignored. |
||
option was used to specify the same error number. Only the last specification is effective. |
||
The license manager is not installed. Install the correct license manager. |
||
The evaluation version of version is valid for the remaining number days. After that, link size limit (256 Kbyte) will be applied. Please consider purchasing the product. |
||
Paid license of "version" is not found, and the evaluation period has expired. Please consider purchasing the product. |
||
The symbol name or section name specified in option cannot be found. name specification is ignored. |
||
"name" in option "option" conflicts between symbol and section |
||
name specified by the option option exists as both a section name and as a symbol name. |
||
The symbol specified by option has already been defined. Processing is continued without any change. |
||
Invalid address value specified in option "option" : "address" |
||
address specified by option is invalid. address specification is ignored. |
||
The "-output" option does not accept specification of a section that has no initial value. |
||
section has no addresses specified for it. section will be located at the rearmost address. |
||
Specify the address of the section using the rlink option "-start". |
||
Address cannot be assigned to absolute section "section" in start option |
||
section is an absolute address section. An address assigned to an absolute address section is ignored. |
||
Section address in start option is incompatible with alignment : "section" |
||
The address of section specified by the start option conflicts with memory boundary alignment requirements. The section address is modified to conform to boundary alignment. |
||
Section attribute mismatch in rom option : "section1","section2" |
||
The attributes and boundary alignment of section1 and section2 specified by the rom option are different. The larger value is effective as the boundary alignment of section2. |
||
Load address overflowed out of record-type in option "option" |
||
A record type smaller than the address value was specified. The range exceeding the specified record type has been output as different record type. |
||
Cannot fill unused area from "address" with the specified value |
||
Specified data cannot be output to addresses higher than address because the unused area size is not a multiple of the value specified by the space option. |
||
The section specified in option does not have an externally defined symbol. |
||
Failed to write type of output code to the output file. The output file may not contain the address to which type of output code should be output. |
||
Area of "FIX" is within the range of the area specified by "cpu=<attribute>" :"<start>-<end>" |
||
In the cpu option, the address range of <start>-<end> specified for FIX overlapped with that specified for another memory type. The setting for FIX is valid. |
||
Section "section name" specified in option "option" is ignored |
||
option specified for the section newly created due to -cpu=stride is invalid. |
||
Input file file1 was overwritten. A backup copy of the data in the previous version of file1 was saved in file2. |
||
Section "section-name" ID(value="number") in "file-name" is reserved |
||
There are numbers that were assigned to be reserved in the section information in the input file. The "number" specification will be ignored. Check if the compiler and assembler versions are correct. |
||
There is no debugging information in the input files. The "option" has been ignored. |
||
Check whether the relevant option was specified at compilation or assembly. |
||
No link-time(inter-module) optimization information is present in the input files. The optimize option has been ignored. |
||
Check whether the goptimize option was specified at compilation or assembly. |
||
No stack information is present in the input files. The stack option is ignored. If all input files are assembler output files, the stack option is ignored. |
||
An unsupported section was present in file. section has been ignored. |
||
Debugging information in file is not dwarf2. The debugging information has been deleted. |
||
The symbol named symbol is duplicated. The symbol in the first file input is given priority. |
||
Sections with the same name but different boundary alignments were input. Only the largest boundary alignment specification is effective. |
||
Sections with the same name but different attributes were input. If they are an absolute section and relative section, the section is treated as an absolute section. If the read/write attributes mismatch, both are allowed. |
||
Common symbols or defined symbols with different sizes were input. A defined symbol is given priority. In the case of two common symbols, the symbol in the first file input is given priority. |
||
Section alignment in option "aligned_section" is small : "section" |
||
Since the boundary alignment value specified for aligned_section is 16 which is smaller than that of section, the option settings made for that section are ignored. |
||
Sections with the same name but different boundary alignment values were input. Only the largest boundary alignment specification is effective. The alignment condition at input may not be satisfied. |
||
Optimization is not available when parentheses "( )" are specified in the start option. Optimization has been disabled. |
||
Cannot optimize "file"-"section" due to multi label relocation operation |
||
A section having multiple label relocation operations cannot be optimized. Section section in file has not been optimized. |
||
Input file was compiled with option "smap" and option "map" is specified at linkage |
||
The file with smap specification should not be compiled with the map option specification in the second build processing. |
||
No SYNCP instruction may be allocated at the location of the exception handler for the exception source name. |
||
See "11.4 Tool for Confirming SYNCP Instruction Insertion at the Beginning of Exception Handler". |