This option displays the version information of ccrl.
[Specification format]
- | Interpretation when omitted |
Compilation is performed without displaying the version information of ccrl.
[Detailed description]
- | This option outputs the version information of ccrl to the standard error output.
It does not execute compilation. |
[Example of use]
- | To output the version information of ccrl to the standard error output, describe as: |