This option specifies that a bit field of a type without a signed or unsigned specifier is handled as a signed type.
A bit field of a type without a signed or unsigned specifier as an unsigned type.
This option specifies that a bit field of a type without a signed or unsigned specifier is handled as a signed type. |
To specify that a bit field of a type without a signed or unsigned specifier is handled as a signed type, describe as: |