This option specifies the Japanese/Chinese character code.
[Specification format]
-character_set={none|sjis|euc_jp|utf8|big5|gb2312}
|
- | Interpretation when omitted |
Processing of Japanese/Chinese character encoding is not performed.
[Detailed description]
- | This option specifies the character code to be used for Japanese/Chinese comments and character strings in the input file. |
- | The parameters that can be specified are shown below.
An error will occur if any other item is specified.
Operation is not guaranteed if the specified character code differs from the character code of the input file. |
none
|
Does not process the Japanese and Chinese character code
|
euc_jp
|
EUC (Japanese)
|
sjis
|
SJIS
|
utf8
|
UTF-8
|
big5
|
Traditional Chinese
|
gb2312
|
Simplified Chinese
|
- | An error will occur if the parameter is omitted. |
[Example of use]
- | To specify EUC as the character code to be used for Japanese comments and character strings in the input file, describe as: |
>asrl -character_set=euc_jp -dev=dr5f100pj.dvf main.asm
|