This option output messages of information level.
[Specification format]
- | Interpretation when omitted |
The output of messages of information level is suppressed (It is the same result as when the -nomessage option is specified).
[Detailed description]
- | This option output messages of information level. |
[Example of use]
- | To output messages of information level, describe as: |
>rlink a.obj b.obj -message
|