Everything

 

-SEction_forbid


This option disables optimization for the specified section.

[Specification format]

-SEction_forbid=sub[,sub]...
    sub: [file-name|module-name](section-name[,section-name]...)

 

-

Interpretation when omitted

Optimization for the specified section is not disabled.

[Detailed description]

-

This option disables optimization for the specified section.

-

Specify the file name, module name, and section name for sub.

-

If an input file name or library module name is also specified, the optimization can be disabled for a specific file, not only the entire section.

[Example of use]

-

To disable all optimizations for the .SEC1 section, describe as:

>rlink a.obj b.obj -optimize -section_forbid=(.SEC1)

 

-

To disable all optimizations for the .SEC1 and .SEC2 sections in a.obj. describe as:

>rlink a.obj b.obj -optimize -section_forbid=a.obj(.SEC1,.SEC2)

[Remark]

-

This option is ignored if optimization is not applied at linkage.

-

To disable optimization for an input file with its path name, type the path with the file name.

-

To disable optimization for the mirror destination area, specify the mirror source area.