This option checks whether the output address of a HEX file ranges in internal ROM or the data flash area.
If this option is specified, whether the output address of an Intel HEX file or a Motorola S-record file ranges in internal ROM or the data flash area is checked. If there is data outside of the range of internal ROM or the data flash area, a warning is output. |
To check whether the address of the output data of an Intel HEX file is outside of the range of internal ROM or the data flash area, code as: |