This option specifies the device file name used at linkage.
The information of the device file is not used at linkage.
When this option is omitted, the settings of the user option bytes, the control value for the on-chip debug, and the security ID value become invalid.
An error will occur if the specifications in the device file differ from the CPU core or the use of the division/multiplication and multiply-accumulate unit specified in the compiler, or the CPU core specified in the assembler. |
An error will occur if the mirror area specified in the assembler differs from that specified in the device file. |
If a device file has not been specified, an error is not output even when the section for the saddr variables is located outside of the saddr area. |