2.6.4 Dependence between options
The behavior of the following options varies depending on what other options are specified.
|
-preprocess
|
This option will be invalid if the -P option is not specified at the same time.
At this time, a warning will not be output.
|
|
-o
|
If the -P, -S, or -c option is specified at the same time, then the generated file types will be a preprocessed file, assembly source file, or object file.
|
|
-g
|
If the -O option is specified at the same time, debug information may not be output in source line units due to optimization effects.
|
|
-Oinline_level
|
If this option is specified at the same time with the -merge_files option, inline expansion may be performed between files.
|