3.3.7
Address overlap information
The overlapped combine source files, and the start and end addresses and size of the continuous range data are output.
The output example of the address overlap information is shown below.
*** Conflict information ***
(1) (2) (3) (4)
FILE START END SIZE
Conflict 1
00000200 00000213 14
sample1.mot
sample2.mot
|
|
|
|
|
|
Overlapped combine source file name
The overlapped combine source file name is output.
|
|
|
Start addresses of overlapped range data
The start addresses of the overlapped range data are output.
This is expressed in a hexadecimal number.
|
|
|
End addresses of overlapped range data
The end addresses of the overlapped range data are output.
This is expressed in a hexadecimal number.
|
|
|
Size of overlapped range data
The size of the overlapped range data is output (in byte units).
This is expressed in a hexadecimal number.
|