Everything
Everything
top
Compiler
COMPILER LANGUAGE SPECIFICATIONS
Extended Language Specifications
4.2
Extended Language Specifications
This section explains the extended language specifications supported by the CC-RL.
To the latest version of this page
Differences Information
Previous Topic
Casting far address to near address and then converting to far address
Next Topic
Reserved words
Table of Contents
Basic Language Specifications
Extended Language Specifications
Reserved words
Macro
C99 language specifications supported in conjunction with C90
#pragma directive
Binary constants
Using extended language specifications
Embedded functions