Returns the low-order 8-bit value of a term.
[Function]
Returns the value of the lower-order eight bits among the 32 bits of a term.
[Application example]
MOV A, #LOW(0x1234) ; (1)
|
(1) | By executing a MOV instruction, this operator loads the low-order 8-bit value "0x34" of the expression "0x1234" to A register. |